Part Number: TMS320F28379D
Other Parts Discussed in Thread: SFRA, , C2000WARE
Hi,
We were able to run the SFRA library on the CPU1 of TMS320F28379D, now we want to run the library on CPU2, for that, I removed the library changes from CPU1 and did the same changes on CPU2 (init, linker, etc.), the software builds fine but when we start the SFRA the freqIndex doesn't get incremented by the SFRA_F32_runBackgroundTask() function. I checked with a breakpoint to confirm this routine is getting called.
Note we are not using the GUI but we can extract the data from the SFRA arrays and we can also monitor how the inject function works when we ran SFRA on CPU1. I was expecting SFRA can run on CPU2 with the same changes. We are NOT trying to run SFRA at the same time from CPU1 and CPU2, I'm not sure if it is possible.
Thanks,
Gabriel