Part Number: TMS320F2808
Other Parts Discussed in Thread: UNIFLASH
Hi,
we have ordered 20 nos of TMS320f2808 controller from mouser in that only 5 got working perfectly with same software in same custom made hardware.
we are loading same firmware (*.out) file using Uniflash with help of XDS100v3 (Olimex) in all controllers and tried in different boards having same hardware design then we found that only some of the controllers working fine without error.
Hardware has error led indication for controller. if error happen the CAN communication gets fails. We are using 2 CAN in this project.
Board 1 is tested Successfully without an error. Board 2 showing error indication. so we replaced the Board 1 TMS controller with Board 2 TMS controller and reprogrammed it.
But still it showing error indication led and CAN Communication gets failing. But if we replace the controller with Tested Ok TMS which also has the same firmware it working fine in Board 1 and Board 2.
Can any one help in this topic.?
We are Loading same Firmware (*.out ) file in all controller.
_Nikhil