Part Number: TMS320F28035
Other Parts Discussed in Thread: CC2640, , TM4C1294NCPDT
Hi champs,
Now my customer want to use an onboard XDS110 (on CC2640 LaunchPad) to program their self-designed TMS320F28035 circuit board. But there are some questions.
①
The JTAG implementation on the onboard XDS110 is cJTAG and the F28035 needs standard JTAG, so we need to drive TRSTn signal manually. The specific operation is to manually connect the TRST signal to the VDDIO level when preparing to connect. This method does work, but the customer thinks that the manual connection method is inconvenient, and the they still hopes to control the TRST signal through the emulator.
But I checked the schematic diagram of onboard XDS110, and did not find the TEST that can be used for connection.
We have checked the e2e link below as a solution. According to the user manual of XDS110, the customer executes the commands marked in blue in the figure, and the phenomenon currently seen by customer is that the emulator's indicator light is flickering. According to the reply in the link below, pin31 should have a level change, but the phenomenon currently seen by customer is that there is no level change.

So could you please give me some suggestions about how to connect TRST signal by using onboard XDS110?
②
And by the way, could you please give me some suggestions about connection of onboard XDS110 and F28335? F28335 need to connect EMU0 and EMU1, just connect the TRST signal to the VDDIO doesn't work.
Thanks a lot!
BR
Julia