Part Number: TMS320F280049C
Hello:
I want to get the "bin file" for upgrade,So I add the below in the post-build step of the CCS.
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
"${CCS_INSTALL_DIR}/utils/tiobj2bin/tiobj2bin.bat" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin"
"${CG_TOOL_ROOT}/bin/ofd2000.exe""${CG_TOOL_ROOT}/bin/hex2000.exe" "${CCS_INSTALL_DIR}/utils/tiobj2bin/mkhex4bin.exe"
--------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
So I get the bin file,but the bin file size is 944kb,it is larger than out file。I check the bin file, The address 0x0~0xe4000 fill the 0x0.
How can i get the bin file on the F280049 project?
CCS Version: 10.2.0.00009
Please Help me asap...
Best regard.