This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: C2000_ware: F28002X

Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE

Hello TI

I am working on TMS320F28035, I have noticed in C2000 ware, there weren't any examples related to F28003X, but fortunately, I have found the F28002X which is the same piccolo family. I have tried to run the epwm file from there but it gives me an error "Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.3.0.00042)" 

The objective is to use this epwm file for the variable frequency ranges from 10 kHz to 800 Khz.

 

Thanks

RG