Hi,
What is the maximum analog signal frequency, that can be measured/converted using the internal 16-bit ADC?
Thanks,
Alen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What is the maximum analog signal frequency, that can be measured/converted using the internal 16-bit ADC?
Thanks,
Alen
Alen,
The maximum frequency is up to the system requirements. Each 16b-capable ADC can convert at 1.1-MSPS:

From a theoretical Nyquist standpoint, the system can sample a (1.1-MSPS / 2) = 550-kHz input signal with proper signal buffering.
-Tommy