Part Number: TMS320F28374D
Other Parts Discussed in Thread: SYSCONFIG
I'm using the following instruction to generate "syscfg" folder for CLB:
${NODE_TOOL} "${CLB_SYSCFG_ROOT}/dot_file_libraries/clbDotUtility.js" "${CLB_SYSCFG_ROOT}" "${BuildDirectory}/syscfg" "${BuildDirectory}/syscfg/clb.dot"
Is there a way to generate this not in "Debug" folder, but in application code?
I've tried the following:
${NODE_TOOL} "${CLB_SYSCFG_ROOT}/dot_file_libraries/clbDotUtility.js" "${CLB_SYSCFG_ROOT}" "${PROJECT_ROOT}/syscfg" "${PROJECT_ROOT}/syscfg/clb.dot"
But it complains:
makefile:510: recipe for target 'post-build' failed
var Module=typeof Module!=="undefined"?Module:{};var moduleOverrides={};var key;for(key in Module){if(Module.hasOwnProperty(key)){moduleOverrides[key]=Module[key]}}Module["arguments"]=[];Module["thisProgram"]="./this.program";Module["quit"]=(function(status,toThrow){throw toThrow});Module["preRun"]=[];Module["postRun"]=[];var ENVIRONMENT_IS_WEB=false;var ENVIRONMENT_IS_WORKER=false;var ENVIRONMENT_IS_NODE=false;var ENVIRONMENT_IS_SHELL=false;if(Module["ENVIRONMENT"]){if(Module["ENVIRONMENT"]==="WEB"){ENVIRONMENT_IS_WEB=true}else if(Module["ENVIRONMENT"]==="WORKER"){ENVIRONMENT_IS_WORKER=true}else if(Module["ENVIRONMENT"]==="NODE"){ENVIRONMENT_IS_NODE=true}else if(Module["ENVIRONMENT"]==="SHELL"){ENVIRONMENT_IS_SHELL=true}else{throw new Error("Module['ENVIRONMENT'] value is not valid. must be one of: WEB|WORKER|NODE|SHELL.")}}else{ENVIRONMENT_IS_WEB=typeof window==="o