Part Number: TMS320F28069
I have built a buck converter based on the TMS320F28069 MCU as its controller, I've implemented the 3P3Z module, calculated the control coefficients and inserted them into my code, the issue is that if I use a crossover frequency higher than 1KHz, the control coefficients become larger than 31.999999 which is the limit for the Q26 numbers.
the coefficients become this big because my output is 12 volt so I have a big divider ratio. and the external reference for the ADC is also 3.3V max
is there a work around this issue?