Part Number: TMS320F28379D
Hi all,
As I add more and more codes I often have the error "program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section." .
I am building my program into RAM, at the beginning I was manually changing the cpu1.cmd by increasing the length of RAMLS5 and 6 and then I was able to compile but now I am at a point where I need to increase RAMD0 | RAMD1 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 but when I try to increase them, either I still have an error or it starts another error in RAMLS4 too small ect...

What is the point of choosing manually the length memory when I am not trying to optimize my code?
I am really surprised, my program is not complex, I am reading some stuff on SPI and try to send them to UART...
I checked and try to ON/OFF gen_func_subsections but it did not do anything.

So my question is, do you have a way to automatically size the memory without of worried about that kind of stuff?
Thank you