Part Number: SM320F28335-EP
Other Parts Discussed in Thread: TMDSCNCD28335,
Dear Ti support Team,
Checking the F28335controlCARD HWDevPkg PGF [R1.0] documentation, especially the TMDSCNCD28335 document number, where F28335 PGF/PTP microcontroller is used, I've noticed the integration of Ferrites on all power supply pins: L1-L18. The Ferrites together with C28 & C29 are creating a very efficient Low-Pass Filter for blocking the uC EMI noise, to be coupled back into the Power Supply lines.
In the current design, we plan to use the SM320F28335-EP microcontroller, and we would like to know the effects of Ferrites removal - on Electromagnetic Emission Noise.
1) Are these Ferrites mandatory to be used with SM320F28335-EP operating at 150MHz internal Clock ?
2) Are these Ferrites necessary on all Supply Pin Groups - VDIO33 / VDD18 / VDADC18 ?
3) In what frequency range these Ferrites are very efficient? Do you have some EMI results from the Demo Board, with / without Ferrites ?
Thank you for your support,
Dragos