This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Query Regarding TMS320F28069 Based Hardware Designing

Hello,

If i use External 10 or 20 Mhz Oscillator having 10 ns rise & fall time. And using that i generate 80 MHz frequency than is there any problem with device operation?

If i used external reference IC for ADC than what is the input current requirement for VREFHI pin.

what type of care required if i use internal Temperature Sensor section using ADC?.

 

Regards,

Yashpal