Part Number: LAUNCHXL-F28379D
Hello,
I have a couple of questions regarding the ADC's on the Launchpad above.
First of all, in the ADCD, there is an additional differential operational amplifier on board. What is the purpose of this? If you can set up the ADC to perform differential conversions, why include an additional differential amplifier prior to the MCU?
Second of all, looking through the documentation for this board, there doesn't seem to be any unity gain buffers/filter components before the input signals are passed to the ADC sensor inputs, even though TI have a document detailing how you need these to provide an ideal driving source to the ADC's. Why is this not included, and should it be designed externally to provide best ADC performance?
In a previous question I asked about providing a precision voltage reference external for the ADC's, and was told this is possible using the analog 14/15 input pins. That is fine. However, the differential amplifier in the ADCD has its own voltage reference. Does this mean you can't use an external precision reference, and does this only apply to the differential input for ADCD?
Best regards,
Joel