This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are developing using HRPWM of your microcomputer F280025.
Please tell me about the following files of C2000Ware.
\C2000Ware_4_00_00_00\libraries\calibration\hrpwm\f28002x\include\sfo_v8.h
Is 4 in "#define PWM_CH_MAX 4" on line 57 of the above file a fixed number that cannot be changed?
If it cannot be changed, can F28002x have high resolution only for the following PWM?
- PWM1A
- PWM1B
- PWM2A
- PWM2B
- PWM3A
- PWM3B
- PWM4A
- PWM4B
Thank you for your reply.
Tatsuya
Hi Tatsuya,
Every controller has a limited number of HRPWM channels. For F280025C, the maximum number of modules that can be used is 4, EPWM1-4 as you rightly pointed out.
You can find the information about the number of HRPWM channels in the device datasheet. For F280025C, you can check here: TMS320F280025 datasheet | TI.com
Thanks,
Aditya
Hi Aditya,
Thanks a lot.
Your answer solved my problem.
Thank you for your help.
Tatsuya