Part Number: TMS320F28335
Dear Sir,
I am trying to control two converters using a single DSP.
Converter 1: Three-phase active front end converter(fsw=10kHz) ----sampling frequency= 10kHz(100us)
Converter 2: DC-DC phase shift full bridge converter ( fsw= 50kHz)---- sampling frequnecy= 50 kHz(20 us)
I have implemented ADC in a dual sequence mode where:
SEQ1= Converter 1, SEQ2= Converter 2
When SEQ1 ISR is called:( 100us sampling)
the ADC value of Conv1 is read from the result register only.
When SEQ2 ISR is called:(20us sampling)
1. the ADC value of Conv2 is read from the Result register
2. control loop calculation for Conv1
3. control loop calculation for Conv2
In my opinion, this approach will work fine if SEQ2 ISR operates under less than 20us. On the other hand, writing code for control loop calculation for such time constraint is a challenge in itself.
I am interested to know if there is a better way to approach this problem.
Please let me know if you need any more information.