Other Parts Discussed in Thread: TMDSDOCK28335
Hi,
when I am using TMDSDOCK28335 with USB power, I am able to use it till I connect oscilloscope probe, the moment I connect probe, I get below error. Any idea why it should happen..???
Error connecting to the target:
Error 0x80000240/-151
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.
SC_ERR_POD_OPEN <-151>
This utility failed to open the adapter for a custom emulator.
The adapter returned an error.
I/O Port = 0
Board Name: F28335 XDS100 USB Emulator
Cpu Name: TMS320C2800_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.