This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: Debugging ti.ramfunc with DCSM enabled

Part Number: TMS320F28377S

I am starting work on a project which uses ti.ramfunc sections to manage flash erase, write operations however when I debug the project in code composer studio all the code assiged to ti.ramfunc sections reads back as zeros and execution halts. 

The project uses the DCSM however I have configured the CSMPSWD settings in the Debug Configuration->Target->Flash Settings->CSMPSWD as well as Project->Properties->Debug->Flash Settings and Code Composer is able to erase the flash and run the program however when it reaches the RamFunc all the values are zero and decode as ITRAP0 (see image below).

Is there a specific debug configuration required to debug a project in this configuration? 

Thanks in advance