Part Number: TMS320LF2406A
Hi Expert,
My customer face an issue that their on-sale product may have possibility that fail to do SCI communicate after running several days. about 6 per 1000 products will have the issue.
below are the details:
1. MCU did not go to illegal ISR as there have blink light controlled by MCU.
2. it is not a soft error, power off device and repower on, there still have this issue.
3. if they reprogramming the MCU by JTAG with same code, there is no issue, which means the device is not destroyed.
4. Cross check test: remove the MCU and replace a new one, there is no this issue, if put the failed MCU to a new board, there still have the issue.
It is old device, there is no way for customer to use emulator to check related registers and flash content.
any suggestion for this? is it possible that some flash bit was changed unexpectedly because reprogramming the device there will no issue.