This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Comparator Subsystem

Part Number: TMS320F28379D

Hello there
I'm just learning the C2000.

I want to compare a voltage value with a threshold voltage and pull the pwm output to low.
I used the cmpss_asynch_cpu01 code in the c2000 ware device support folder, but I can't see any signal from the pwm outputs on the launchpad. I set the connections as follows;

comp + signal connected = ADCINA2 pin (i connected a potentiometer 0-3.3V)
NEG signal from internal DACH

I don't see any signal when I measure the PWM8B/ GPIO15 output. Where am I missing?
Thanks