Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMDSDOCK28379D, CONTROLSUITE, TMDSCNCD28379D
Hi,
currently, I am using USB to connect to TMDSDOCK28379D and TMDSDOCK28379D and control the external high-frequency converter. More than often communication breaks down when the converter voltage and power increase when I am in the MATLAB Simulink External Mode for Parameter Tuning and Signal Logging with Serial Communication.
I was thinking of adding RS232 and RS485 communication to load applications and monitor data. Maybe this will make the communication more robust?!
There are four SCIs (SCI_A, SCI_B, SCI_C and SCI_D) in Simulink settings and I can assign various GPIOs from the list to RX and TX.
1. How the system knows which SCI is used? There is an option 'Pin Assignment: None' in the settings for each SCI RX/TX; is this the only way to turn off the each channel SCI communication? Can I have more communications channels on 'stand-by' so I can try them all while the system is running? I would like to use other SCIs, e.g., SCI_B for RS232 and SCI_C for RS485, but not sure how the system will know which one is active
2. I have created a basic schematics for RS232 and RS485. Will this work or do I need to add something?

Thank you in advance