Part Number: TMS320F28069
Because DMA is supposed to have access to the ePWM registers, I assumed I could clear the cycle-by-cycle trip flags at CTR=0 using DMA. I set up DMA, use a static global in L5-L8 memory as source, and attempt to use EPwm4Regs.TZCLR as source, however this does not clear the flags. I checked the following things:
- When writing the global variable to TZCLR by software, the flags are cleared as expected
- When writing to a destination in L5-L8 RAM, the global variable is copied by DMA as expected
I have no idea what else I can check. Maybe it has something to do with the TZCLR register being EALLOW protected? Anyone with an idea what is going wrong here? I set up the channel with a function as follows:
int16 CopyNextCycle(Uint32 Src, Uint32 Dst, Uint16 Size)
{
Uint16 ChNr = 0;
while (ChannelsInUse[ChNr])
{
ChNr++;
if (ChNr > 5) {
return 1;
}
}
ChannelsInUse[ChNr] = 1;
GET_REG_LOCK;
ChannelPtr[ChNr]->MODE.all = 0;
ChannelPtr[ChNr]->MODE.bit.CONTINUOUS = 0;
ChannelPtr[ChNr]->MODE.bit.PERINTE = 1;
ChannelPtr[ChNr]->MODE.bit.PERINTSEL = 18; // Triggered by PWM module 2 SoC A
ChannelPtr[ChNr]->MODE.bit.CHINTE = 1; // Generate interrupt (to mark channel as 'not anymore in use')
ChannelPtr[ChNr]->MODE.bit.CHINTMODE = 1; // Generate interrupt at end of transfer
ChannelPtr[ChNr]->BURST_SIZE.all = Size;
ChannelPtr[ChNr]->SRC_BURST_STEP = 1;
ChannelPtr[ChNr]->DST_BURST_STEP = 1;
ChannelPtr[ChNr]->TRANSFER_SIZE = 1;
ChannelPtr[ChNr]->SRC_ADDR_SHADOW = Src;
ChannelPtr[ChNr]->DST_ADDR_SHADOW = Dst;
ChannelPtr[ChNr]->CONTROL.all = 0;
ChannelPtr[ChNr]->CONTROL.bit.RUN = 1;
RELEASE_REG_LOCK;
return 0;
}
Then I call this function with the static variable as source, and the TZCLR register as destination, as follows:
CopyNextCycle((Uint32)&CbCTripFlagClear, (Uint32)&(EPwm4Regs.TZCLR), 1);