Part Number: TMS320F28377D
ADC is assigned to cpu01 and the EOC triggers adca1 interrupt in cpu01. Can I also create an adca1 interrupt in cpu02 based on the same EOC as cpu01? How do I both initialize and acknowledge/clear this interrupt in cpu02?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377D
ADC is assigned to cpu01 and the EOC triggers adca1 interrupt in cpu01. Can I also create an adca1 interrupt in cpu02 based on the same EOC as cpu01? How do I both initialize and acknowledge/clear this interrupt in cpu02?
Rachael,
Yes, the ADC interrupt signal is simultaneously available to the respective PIE module of both CPUs.
With the ADC assigned to CPU1:
-Tommy