Part Number: TMS320F28379D
Hi All,
Our company is working on ti28379d module with ccs 10.3.1 , We tried to apply DELAY_US function but it shows two types of behavior in the program
1. Works fine:-When we use it with f2837xd source and header files , debugged in RAM then it gives correct result.(bit field approach)
2. Error:- While running the program in flash along with some driverlib files it is giving error & is not executable.(bit field+driverlib approach)
kindly look into the issue and help us out to resolve it.
Drishti Mittal