Part Number: TMS320F28027
Dear Teams,
My customer is using TMS320F28027 EVM, and they have following requirement. Could you help give some suggestions here?
They used LAUNCHXL-F28027, and want to change the ADC's clock to 1Mhz. Their current setting is:
1. Window size to 7
2. SoC set to 2
3. Clock frequency is 50Mhz
4. ePWM set to 50
Thus, the output should be 1Mhz. However, they connect the ePWM to the GPIO and test it with oscillscope, then they found the actual clock frequency only has 120kHz.
Could you help give some suggestions here?
Thanks!
Dylan