Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: C2000WARE
Hi, I'm using F28035 on my TMDSHVMTRPFCKIT, trying to upload a practice program controlling the blinking sequence of the LEDs on the TMDSHVMTRPFCKIT board.
When I build the program onto the control card, I can run the program but when I turn the control supply off and back on again, the program on the control card vanishes.
I surfed the internet for solution and found boot from flash option which enables program uploaded onto the card to be run without connection to the computer. Well, I checked the switch configuration on the control card and all is set as default.
How can I keep the uploaded program on the control card even after control supply is turned off and back on?
thank you in advance.