Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: UNIFLASH
I want to upload my code from psim to board. How can i connect rs-232 to TMDSHVMTRPFCKIT? i cant find isolated rx and tx port on the board.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSHVMTRPFCKIT
Other Parts Discussed in Thread: UNIFLASH
I want to upload my code from psim to board. How can i connect rs-232 to TMDSHVMTRPFCKIT? i cant find isolated rx and tx port on the board.
This kit includes an onboard XDS100 emulation connection to interface with the C2000 MCU as well as download code via Code Composer or Uniflash. Assuming PSIM is generating a coff(.out) file, you can use the emulation connection to download the code to the C2000 that is in the kit.
Best,
Matthew
Thank you for your reply. And another question i want to set switch s1 on F28335 control card to off position. How can i change it from on to off. I dont know how to set it.
This should be a 1 position DIP switch on the control CARD, if you don't see this you may have an older revision of the control CARD. Can you see if there is a sticker or silk screen indication of the revision of your controlCARD?
Best,
Matthew