Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
1. if i want to be able to update firmware from usb driver, which boot mode should be selected: sci/spi/i2c/parallel?
2. is there other IC needed in between the microcontroller and the usb connector?
3. is there a example i can refer to accomplish this task?
Thanks!