Part Number: TMS320F2808
I have come across a behavior I cannot explain. It seems that MSGID.bit.AAM only works if the defined transmit mailbox is 16 - 31.
The example below works as I can send a CAN message to the F2808 with ID of 5 and I get an auto answer. Note that MBOX2 is Rx and MBOX28 is Tx
However, if I make MBOX28 Rx and MBOX2 Tx as well as "ECanaRegs.CANMD.all = 0xFFFF0000;" to swap Rx an Tx directions and use CANTA.bit.TA2, I no longer get an auto answer. I have tired other MBOX combinations but only Tx mailboxes in the 0 - 15 range work. Any thoughts?
// Receive
ECanaMboxes.MBOX2.MSGID.bit.STDMSGID = 5;
ECanaMboxes.MBOX2.MSGID.bit.IDE = 0;
ECanaMboxes.MBOX2.MSGID.bit.AAM = 0;
ECanaMboxes.MBOX2.MSGCTRL.bit.DLC = 8;
// Transmit
ECanaMboxes.MBOX28.MSGID.bit.STDMSGID = 5;
ECanaMboxes.MBOX28.MSGID.bit.IDE = 0;
ECanaMboxes.MBOX28.MSGID.bit.AAM = 1;
ECanaMboxes.MBOX28.MDL.all = 0x28282828;
ECanaMboxes.MBOX28.MDH.all = 0x28282828;
/* Enable appropriate Mailboxes in CAN-A*/
ECanaRegs.CANME.all = 0xFFFFFFFF;
/* Configure CAN-A Mailboxes as RX (1) and TX (0)*/
ECanaRegs.CANMD.all = 0x0000FFFF;
while(1)
{
do {ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;} // Wait for TA28 bit to be set..
while(ECanaShadow.CANTA.bit.TA28 == 0);
if(ECanaShadow.CANTA.bit.TA28)
{
ECanaShadow.CANTA.all = 0;
ECanaShadow.CANTA.bit.TA28 = 1; // Clear TA28
ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;
// Update the mailbox data
ECanaMboxes.MBOX28.MDL.all += 3;
}
}