Part Number: TMS320F280025C
Hi everyone,
Excuse me but I have exchanged on this subject with Subrahmanya , but the topic has closed and I have others questions.
You can see a screen shot. Why when I set phase = 120° ePWM2 is OK with correct phase shift with ePWM1 and ePWM3 isn't OK ? Can you explain me more please ? If I understand correctly we must reverse the direction by TBPHSDIR on UP and DOWN count but I can't do it.
Thanks
My code :
void set_phase(uint32_t base, uint16_t phi)
{
uint16_t phase;
if(base == myEPWM2_BASE)
{
//EPWM_setCountModeAfterSync(base, EPWM_COUNT_MODE_UP_AFTER_SYNC);
phase = ((float)phi * HWREGH(base + EPWM_O_TBPRD) * 2 / 360); // *2 to adapt scale on UP and DOWN Count mode
}
if(base == myEPWM3_BASE)
{
//EPWM_setCountModeAfterSync(base, EPWM_COUNT_MODE_UP_AFTER_SYNC);
phase = ((float)phi * 2 * HWREGH(base + EPWM_O_TBPRD) * 2 / 360);
}
EPWM_enableSyncOutPulseSource(base, EPWM_SYNC_OUT_PULSE_ON_SOFTWARE);
EPWM_forceSyncPulse(base);
EPWM_setPhaseShift(base, phase);
EPWM_setTimeBaseCounter(base, phase);
EPWM_enablePhaseShiftLoad(base);
}float PWM_Freq_TBCLK = (float) SYSCLK / (PWM_HIGHSPEED_PRESCALER * PWM_PRESCALER); *TBCLK = 1. / PWM_Freq_TBCLK; PWM_period = 1. / PWM_FREQ; time_FED_RED = (FED + RED) * 0.000001; PWM_period += time_FED_RED; *TBPRD_boost_3 = PWM_Freq_TBCLK / (PWM_FREQ * 2); *CMPA_boost_3 = ((float) (100 - duty_boost_3) / 100) * (*TBPRD_boost_3);
void epwm_init(uint32_t base)
{
float PWM_TBPRD_1;
float PWM_TBPRD_2;
float PWM_TBPRD_3;
float PWM_CMPA_1;
float PWM_CMPA_2;
float PWM_CMPA_3;
EPWM_ClockDivider PWM_PARAM_PRESCALER;
EPWM_HSClockDivider PWM_PARAM_HIGHSPEEDPRESCALER;
float TBCLK;
if(base == myEPWM1_BASE)
{
get_pwm_clock_from_freq(base , &PWM_TBPRD_1 , &PWM_TBPRD_2 , &PWM_TBPRD_3 , &PWM_CMPA_1 , &PWM_CMPA_2 , &PWM_CMPA_3 , &PWM_PARAM_PRESCALER , &PWM_PARAM_HIGHSPEEDPRESCALER, &TBCLK);
// Parameters
EPWM_setTimeBasePeriod(base, (uint16_t)PWM_TBPRD_1);
EPWM_setCounterCompareValue(base, EPWM_COUNTER_COMPARE_B, (uint16_t)PWM_CMPA_1);
EPWM_setPhaseShift(base, 0U);
EPWM_disablePhaseShiftLoad(base);
EPWM_setTimeBaseCounter(base, 0U);
EPWM_enableSyncOutPulseSource(myEPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_CNTR_ZERO);
}
else if (base == myEPWM2_BASE)
{
get_pwm_clock_from_freq(base , &PWM_TBPRD_1 , &PWM_TBPRD_2 , &PWM_TBPRD_3 , &PWM_CMPA_1 , &PWM_CMPA_2 , &PWM_CMPA_3 , &PWM_PARAM_PRESCALER , &PWM_PARAM_HIGHSPEEDPRESCALER, &TBCLK);
// Parameters
EPWM_setTimeBasePeriod(base, (uint16_t)PWM_TBPRD_2);
EPWM_setCounterCompareValue(base, EPWM_COUNTER_COMPARE_A, (uint16_t)PWM_CMPA_2);
EPWM_setPhaseShift(base, 0U);
EPWM_disablePhaseShiftLoad(base);
EPWM_setTimeBaseCounter(base, 0U);
EPWM_setSyncInPulseSource(base, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
set_phase(base, PHI);
}
else if(base == myEPWM3_BASE)
{
get_pwm_clock_from_freq(base , &PWM_TBPRD_1 , &PWM_TBPRD_2 , &PWM_TBPRD_3 , &PWM_CMPA_1 , &PWM_CMPA_2 , &PWM_CMPA_3 , &PWM_PARAM_PRESCALER , &PWM_PARAM_HIGHSPEEDPRESCALER, &TBCLK);
// Parameters
EPWM_setTimeBasePeriod(base, (uint16_t)PWM_TBPRD_3);
EPWM_setCounterCompareValue(base, EPWM_COUNTER_COMPARE_A, (uint16_t)PWM_CMPA_3);
EPWM_setPhaseShift(base, 0U);
EPWM_disablePhaseShiftLoad(base);
EPWM_setTimeBaseCounter(base, 0U);
EPWM_setSyncInPulseSource(base, EPWM_SYNC_IN_PULSE_SRC_SYNCOUT_EPWM1);
set_phase(base, PHI);
}
//EPWM_setTimeBaseCounter(base, 0U);
EPWM_setTimeBaseCounterMode(base, EPWM_COUNTER_MODE_UP_DOWN);
EPWM_setClockPrescaler(base, PWM_PARAM_PRESCALER, PWM_PARAM_HIGHSPEEDPRESCALER);
// Set up shadowing
EPWM_setCounterCompareShadowLoadMode(base, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO);
// Set actions
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(base, EPWM_AQ_OUTPUT_B, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
// Trip zone
// Configure ePWM1x to output low on TZx TRIP
EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW);
EPWM_setTripZoneAction(base, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW);
// Trigger event when DCBH is high
EPWM_setTripZoneDigitalCompareEventCondition(base, EPWM_TZ_DC_OUTPUT_B1, EPWM_TZ_EVENT_DCXH_HIGH);
// Configure DCBH to use TRIP4 as an input
EPWM_enableDigitalCompareTripCombinationInput(base, EPWM_DC_COMBINATIONAL_TRIPIN4, EPWM_DC_TYPE_DCBH);
// Enable DCB as OST
EPWM_enableTripZoneSignals(base, EPWM_TZ_SIGNAL_DCBEVT1);
// Configure the DCB path to be unfiltered and asynchronous
EPWM_setDigitalCompareEventSource(base, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL);
// Clear trip flags
EPWM_clearTripZoneFlag(base, EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_OST);
// Calculate delays
get_delays_FED_RED(myEPWM1_BASE, &TBCLK);
get_delays_FED_RED(myEPWM2_BASE, &TBCLK);
get_delays_FED_RED(myEPWM3_BASE, &TBCLK);
}