Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Wrong value in flexible array member

Part Number: LAUNCHXL-F28069M

Hi, 

I'm using the c2000 21.6.0.LTS compiler and I tried both COFF and EABI format, the result was the same.


typedef struct {
    unsigned a;
    unsigned b;
} entry_t;

typedef struct {
    unsigned len;
    entry_t entries[];
} array_t;

const array_t array = {
  .len = 3,
  .entries = {
            { .a = 1,},
            { .a = 2},
            { .a = 3},
  },
};
const unsigned neighbor = 0xabcd;
/**
 * main.c
 */
volatile unsigned va;

volatile unsigned vb;


int main(void)
{
    va = array.entries[2].a;
    vb = array.entries[2].b;
    return 0;
}

I would expect  vb == 0, but after running the code it's actually vb == 0xABCD, the value of neighbor. It looks like the compiler calculates the space for array wrong. Adding a dummy entry at the end of the array would fix the problem.

Best regards,
Simon