Other Parts Discussed in Thread: TMS320F28335, CCSTUDIO
Hi,
I am using ccstudio, TMS320F28335 DSP microcontroller and to explore I generated new library with memcpy_ff.c file and string.h file. I did not include memcpy.c file as part of my library. But I am using memcpy() in my code.
I have few quereis.
1. I did not include sting.h in .c file. But i am using memcpy() in my code. Compiler did not give implicit function usage warning or error saying no memcpy() function.
2. If i debug controll is going to memcpy_ff(). How come if i call memcpy() control is going to memcpy_ff() function. Even there is not prototype of memcpy() in string.h. only prototype of memcpy_ff() is present in string.h
3. Which prototype should i follow. far void* or just void*. Below are the examples i tried.
// memcpy_ff example (No error and calls memcpy_ff() function
{
far void *destination_string = "Vishnu";
const far void *source_string = "Vardhan";
far void *return_string;
unsigned int no_of_char = 5;
return_string = far_memcpy(destination_string, source_string, no_of_char);
if(destination_string == return_string)
{
testArray[3] = TEST_PASS;
}
else
{
testArray[3] = TEST_FAIL;
}
}
// memcpy_ff prototype with memcpy function example (ERROR saying "main.c", line 105: error #169: argument of type "void far *" is incompatible with parameter of type "void *"
{
far void *destination_string = "Vishnu";
const far void *source_string = "Vardhan";
far void *return_string;
unsigned int no_of_char = 5;
return_string = memcpy(destination_string, source_string, no_of_char);
if(destination_string == return_string)
{
testArray[3] = TEST_PASS;
}
else
{
testArray[3] = TEST_FAIL;
asm(" ESTOP0");
}
}
// memcpy prototype with memcpy_ff function example (No error, calls memcpy_ff() function but not memcpy().
{
int buff1[10];
int buff2[10] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10};
int* retVal;
retVal = (int*) far_memcpy(buff1, buff2, sizeof(buff1));
}
// memcpy example (No error but CALLS memcpy_ff() function
{
int buff1[10];
int buff2[10] = {1, 2, 3, 4, 5, 6, 7, 8, 9, 10};
memcpy(buff1, buff2, sizeof(buff1));
}
Thanks & Regards
Vishnu