This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Sysconfig error when using TIDM_HV_1PH_DCAC

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG

Hi Champs,

My customer now is using TIDM_HV_1PH_DCAC to test the project (C2000Ware_DigitalPower_SDK_3_03_00_00\solutions\tidm_hv_1ph_dcac\f2837x\ccs\gridconnectedinvlclfltr\gridConnectedInverterLCLFltr_F2837x).

Both CCS11.0 and Sysconfig have been installed correctly. And when they built the project they got an error as below:

1 gmake: Target 'all' not remade because of errors.      gridConnectedInverterLCLFltr_F2837x                    C/C++ Problem

2 unsupported platforms will not be fixed.gmake: *** [build-1212147823] Error 216  gridConnectedInverterLCLFltr_F2837x                     C/C++ Problem]

The content of the error shows "Node.js is only supported on Windows 8.1", and the customer is using windows7. According to the suggestions in the "error message", NODE_SKIP_PLATFORM_CHECK should be set to 1. But I have no idea about that because I cannot find NODE_SKIP_PLATFORM_CHECK.

As a comparison, if the customer builds the gridConnectedInverterLCLFltr_nonpowerSUITE_F2837x project in the same directory, no error will be displayed. The difference between these two projects is whether Sysconfig is used. I want to know if it is the problem with Sysconfig? Can Sysconfig be used in Windows 7?

Could you please help me to solve this error? Any help would be very thankful.

BR

Julia

  • I think this may be a SysConfig/Node/CCS issue.

  • Hi Nima,

    Many thanks for your reply! So reinstall CCS or Sysconfig can fix it? I did not find any depiction about Sysconfig cannot be used in Windows 7 in the relevant materials. So I wanna cheak with you whether Sysconfig can work on windows 7?

    And I still wanna know what's "Node" means in CCS? Thanks!

    BR

    Julia

  • Julia,

    The short answer is that you need to set the NODE_SKIP_PLATFORM_CHECK environment variable to 1 before starting CCS.

    The longer answer is node is a command line executable that can also execute JavaScript, and that is what the build system uses to invoke the build step for the SysConfig code-generation.  The version of node was updated in CCS 11.0 to a version which doesn't have windows 7 support for every feature, but it does for the features SysConfig uses.  As such, that environment variable will skip the check and allow the SysConfig step to run.

    This is a known issue and will be fixed in 11.2

    Darian