Other Parts Discussed in Thread: TMS320F28034
We use C2000-GANG programmer for flashing 4x TMS320F28034 at the same time (on the same PCB). My question is directed to application C2000-Gang.exe ver. 1.1.5.0
We use Scripting file .c2000gangsf.
Sometimes it happens that programming of one (or more) target(s) is not successful. So the script asks operator whether they want to re-flash again. Even though the re-flash is successful the over all result is FAILED. The status remain FAILED any further attempt until the script is finished. When I restart the script again the programming PASS.
The first picture is simulation of failed programming (with pop-up window). The second picture shows the status after second (third, fourth...) attempt.


So my expectation is that the API is not Can you suggest what to do with this issue.
Below is result file after successful but FAIL second attempt
#( Tue, Nov 23,2021, 12:14:46 )
#Comment: Failed
#RESULTS:
80 A5 1F 00 00 00 90 00 1F 00 0F 0F 0F 0F 0F 0F 0F 00 00 00 00 00 00 00 00 64 00 0F 00 00 00 00 00 64 46 69 6E 69 73 68 65 64 20 20 20 20 20 20
Finished task mask: 001F
Cumulative target mask: 0F
Requested target mask: 0F
Connected target mask: 0F
Erased target mask: 0F
Blank Check target mask: 0F
Programmed target mask: 0F
Verified target mask: 0F
Secured target mask: 00
error_no: 00
VTIO in mV: 3200
Vcc Error target mask: 00
Vcc Cumulative Err mask: 00
JTAG Init Err mask: 00
Already Secured mask: 00
Wrong MCU ID mask: 00