This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: After I2c enables FIFO, RXFFST is always 0 and cannot be read

Part Number: TMS320F28335


Dear team:

In the code of my client, FFST is always 0 in case1, which causes it to get stuck in an infinite loop and cannot read the value. Please tell me what went wrong?

void drv_I2C_read(Uint16 uiPar_Addr,Uint16 recieve_bytes)
{
Uint16 uiaddr;
Uint16 NUM;
NUM = recieve_bytes;
switch(stDrv_I2C.uiread_state)
{
case 0:
uiaddr = uiPar_Addr;

DELAY_US(1000L); // Delay 1ms
I2caRegs.I2CCNT = 1; // Set 1 byte to be transmitted
I2caRegs.I2CDXR = uiaddr;

I2caRegs.I2CMDR.all = FRE + STT + MST + TRX + IRS; // Configure mode register as transmitter mode
DELAY_US(1000L); // Delay 1ms
I2caRegs.I2CCNT = NUM; // Set 1 byte to be transmitted
I2caRegs.I2CMDR.all = FRE + STT + STP_CMD + MST + IRS; // Configure mode register as receive mode
stDrv_I2C.uiread_state = 1;
break;
case 1:
if(I2caRegs.I2CFFRX.bit.RXFFST >= 1) // Confirm 1 byte had been received------------------------------------I'm stuck here.RXFFST always 0
stDrv_I2C.uiread_state = 2;
break;
case 2:
stDrv_I2C.uiread_data.byte.hi = I2caRegs.I2CDRR; // Acquire high byte data bytes
stDrv_I2C.uiread_data.byte.lo = I2caRegs.I2CDRR; // Acquire low byte data bytes
stDrv_I2C.uiread_state = 3;
break;
case 3:
stDrv_I2C.uiread_state = 0; // Reset I2C flow-status flag
stDrv_I2C.uiread_end = 1; // Set I2C END status
break;
default:
break;
}
}

Best regards