Part Number: TMS320F28335
I am trying to do SPI communication with MAX31856 (temperature measurement) using TMS320F28335.
0x0c is transmitted in the first byte
Transmit the remaining 3 bytes 0x00.
The problem is that the values received are not constant and are displayed as 254 or 255.
In my opinion, I think that communication is going on. (It may not be.)
Also, I think there is nothing wrong with the hardware connection.
Below is the code I wrote, I think there is an error in the received value.
What could be causing this?
Thanks for your help.

while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG);
TxData[0]=0x0c;
SpiaRegs.SPITXBUF = (TxData[0]<<8);
while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG);
TxData[1]=0x00; //dummy byte
SpiaRegs.SPITXBUF = TxData[1];
while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG);
TxData[2]=0x00;
SpiaRegs.SPITXBUF = TxData[2];
while(SpiaRegs.SPISTS.bit.BUFFULL_FLAG);
TxData[3]=0x00;
SpiaRegs.SPITXBUF = TxData[3];
for(i=0;i<4;i++)
{
RxData[i] = SpiaRegs.SPIRXBUF;
}