Part Number: TMS320F28069
Other Parts Discussed in Thread: UNIFLASH
Hi,
Customer is encountering error regarding this IC, please see details below.
"I'm working with\ TMS320F28069 and Texas Instruments XDS100v2 USB Debug Probe and I have a problem to program it with PC connected to the USB (like Launch pad ).
Before this I have done a programming with a new code where I have put a new initialization of SCIA and SCIAB. perhaps I have done some mistake in the code but the result is that, now, I cannot reprom the device.
I cannot program it. I tried with UNiflash and it is not possible to erase the flash and to program the device with loadprogram Too.
When I try to erase the Flash (only sector A) the message is :
[1/12/2021 14:46:33] [ERROR] C28xx: Flash Programmer: Error erasing flash memory. Device is locked or not connected. Operation cancelled
When I try to loadprogram the message is :
C28xx: Trouble Halting Target CPU: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Error: (Error -1135 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 8.3.0.00003)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx: GEL: Error while ex
Maynard