Part Number: TMS320F28374S
The default ADC software demo of 2837xS is 12-bit sampling mode, now 16-bit single-end sampling is needed, whether it can be supported, and the software and hardware reference design demo can help provide.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28374S
The default ADC software demo of 2837xS is 12-bit sampling mode, now 16-bit single-end sampling is needed, whether it can be supported, and the software and hardware reference design demo can help provide.
Hi,
Yes, 16-bit in differential mode is also supported on this device. there are no explicit examples for the same at the moment but the existing example can be easily modified by configuring the appropriate mode and acquisition time. Let me know if you face any issues in this.
Thanks
Vasudha