This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Problem in PWM waveform while using ADC

Part Number: TMS320F28379D

I want to generate phase shifted PWM waveform in the following way:

EPWM1A and EPWM1B - Master;

EPWM2A and EPWM2B - Phase shifted from EPWM1 by D1;

EPWM3 SOC A is used for triggering SOC of ADCs.

EPWM4A and EPWM4B is phase shifted from EPWM1 by D;

EPWM5A and EPWM5B is phase shifted from EPWM1 by D+D2.

Four ADCs are used - 

ADCA2 - used for measuring D - Result stored in ADCARESULT0 - Moving average filter of 10 samples - result fed to EPWM4 phase register in interrupt.

ADCB2 - used for measuring D1 - Result stored in ADCBRESULT1 - Moving average filter of 100 samples - result fed to EPWM1 phase register in interrupt.

ADCA3 - used for measuring D2 - Result stored in ADCARESULT2- Moving average filter of 100 samples - result fed to EPWM phase register in interrupt.

ADCB3 - used for measuring Mode current - Result stored in ADCBRESULT3 .

As soon I try to generate PWM waveforms based on ADC's after a certain level, the  noise arrives in PWM waveform which causes the PWM waveform very much shifted in some instants creating problem in hardware. 100 pF is attached near the ADCs as filter. When the hardware is run at open loop, no such phenomenon is observed.

The code is attached as here.

//###########################################################################
//
// FILE:    epwm_deadband_c28.c
//
// TITLE:   Check PWM Dead-Band
//
//! \addtogroup cpu01_example_list
//! <h1> EPWM dead band control (epwm_deadband)</h1>
//!
//! During the test, monitor ePWM1, ePWM2, and/or ePWM3 outputs
//! on a scope.
//!
//! - ePWM1A is on GPIO0
//! - ePWM1B is on GPIO1
//! - ePWM2A is on GPIO2
//! - ePWM2B is on GPIO3
//! - ePWM3A is on GPIO4
//! - ePWM3B is on GPIO5
//!
//! This example configures ePWM1, ePWM2 and ePWM3 for:
//! - Count up/down
//! - Deadband
//!
//! 3 Examples are included:
//! - ePWM1: Active low PWMs
//! - ePWM2: Active low complementary PWMs
//! - ePWM3: Active high complementary PWMs
//!
//! Each ePWM is configured to interrupt on the 3rd zero event.
//! When this happens the deadband is modified such that
//! 0 <= DB <= DB_MAX.  That is, the deadband will move up and
//! down between 0 and the maximum value.
//!
//! View the EPWM1A/B, EPWM2A/B and EPWM3A/B waveforms
//! via an oscilloscope
//
//
//###########################################################################
// $TI Release: F2837xD Support Library v3.12.00.00 $
// $Release Date: Fri Feb 12 19:03:23 IST 2021 $
// $Copyright:
// Copyright (C) 2013-2021 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"



//Defines
#define D12_BUFFER 200
#define D_BUFFER 20
#define EPWM_DB 100

//
//
//
// Globals
//
Uint16 Mode_current;
Uint16 D1;
Uint16 D2;
Uint16 D;
Uint32 D1_adcb1;
Uint32 D2_adcb2;
Uint32 D_adcb3;
Uint16 D1_adcbresult1[D12_BUFFER];
Uint16 D2_adcbresult2[D12_BUFFER];
Uint16 D_adcbresult3[D_BUFFER];
Uint16 indexD12;
Uint16 indexD;



//
// Function Prototypes
//Here for simple DAB we will use EPWM1, EPWM2, EPWM4, EPWM5, EPWM6

void InitEPwm1Example(void);
void InitEPwm2Example(void);
void InitEPwm3Example(void);
void InitEPwm4Example(void);
void InitEPwm5Example(void);

void ConfigureADC(void);
void SetupADCSoftware(void);

__interrupt void adcb2_isr(void);


//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks


// This example function is found in the F2837xD_SysCtrl.c file.
//




    InitSysCtrl();

//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to its default state.
//
    InitGpio();


//
// enable PWM1, PWM2 and PWM3
//
    CpuSysRegs.PCLKCR2.bit.EPWM1=1;
    CpuSysRegs.PCLKCR2.bit.EPWM2=1;
    CpuSysRegs.PCLKCR2.bit.EPWM3=1;
    CpuSysRegs.PCLKCR2.bit.EPWM4=1;
    CpuSysRegs.PCLKCR2.bit.EPWM5=1;

//
// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the F2837xD_EPwm.c file
//
    InitEPwm1Gpio();
    InitEPwm2Gpio();
    InitEPwm3Gpio();
    InitEPwm4Gpio();
    InitEPwm5Gpio();

//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
    DINT;

//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
    InitPieCtrl();

//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
    IER = 0x0000;
    IFR = 0x0000;

//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
    InitPieVectTable();

//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.ADCB2_INT = &adcb2_isr;
    EDIS;   // This is needed to disable write to EALLOW protected registers

//
// Step 4. Initialize the Device Peripherals:
//

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
    EDIS;


    InitEPwm1Example();
    InitEPwm2Example();
    InitEPwm3Example();
    InitEPwm4Example();
    InitEPwm5Example();



//
// Step 5. User specific code, enable interrupts:
// Initialize counters:
//

//
// Enable CPU INT10 which is connected to ADCB2 INT:
//

    IER |= M_INT10;

//
// Enable ADCB2 INTn in the PIE: Group 10 interrupt 6
//

    PieCtrlRegs.PIEIER10.bit.INTx6 = 1;

//
// Enable global Interrupts and higher priority real-time debug events:
//
    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM


//
//
// Initialize results buffer
//
    for(indexD12 = 0; indexD12 < D12_BUFFER; indexD12++)
    {
        D1_adcbresult1[indexD12] = 0;
        D2_adcbresult2[indexD12] = 0;
    }
    for(indexD = 0; indexD < D_BUFFER; indexD++)
    {
        D_adcbresult3[indexD] = 0;
    }
     indexD12 = 0;
     indexD   = 0;
     D1_adcb1 = 2500;
     D2_adcb2 = 2500;
     D_adcb3 = 10;
     D1 = 2500;
     D2 = 2500;
     D = 10;

// Setup ADC

     ConfigureADC();
     SetupADCSoftware();

//
    //start ePWM
    //
    EPwm3Regs.ETSEL.bit.SOCAEN = 1;  //enable SOCA
    //EPwm3Regs.ETSEL.bit.SOCBEN = 1;  //enable SOCB
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; //unfreeze, and enter down count mode
    //EPwm1Regs.ETSEL.bit.SOCAEN = 1;  //enable SOCA
    //EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; //unfreeze, and enter down count mode

    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
    EDIS;
//
// Step 6. IDLE loop. Just sit and loop forever (optional):
//
    do
        {
            //
            // Wait while ePWM causes ADC conversions.
            // ADCA1 ISR processes each new set of conversions.
            //
        }
        while(1);
}


//
// adcb2_isr
//
__interrupt void adcb2_isr(void)
 {
     Uint16 i;

     D_adcbresult3[indexD++] = AdcaResultRegs.ADCRESULT0;
     D1_adcbresult1[indexD12] = AdcbResultRegs.ADCRESULT2;
     D2_adcbresult2[indexD12++] = AdcaResultRegs.ADCRESULT1;
     Mode_current  = AdcbResultRegs.ADCRESULT3;

     if (indexD12 >= D12_BUFFER)
     {   indexD12 = 0;

         D1_adcb1 = 0;
         D2_adcb2 = 0;

         for(i = 0; i < D12_BUFFER; i++)
         {D1_adcb1 = D1_adcb1 + D1_adcbresult1[i];
          D2_adcb2 = D2_adcb2 + D2_adcbresult2[i];
         }
     }

         D1 = D1_adcb1*0.005*0.916;
         D2 = D2_adcb2*0.005*0.916;



    //Limiter for D1 and D2
    if (D1 < 1000)
    {D1 = 1000;
    }
    else if (D1 > 2500)
    {D1 = 2500;
    }

    if (D2 < 1000)
    {D2 = 1000;
    }
    else if (D2 > 2500)
    {D2 = 2500;
    }


     if (indexD >= D_BUFFER)
      {  indexD = 0;

     D_adcb3 = 0;

         for(i = 0; i < D_BUFFER; i++)
           {D_adcb3 = D_adcb3 + D_adcbresult3[i];
           }
      }

      // 0.36632 is the calculated factor required to match the adcin results and TBPHS register
     if (Mode_current > 1000)
     { D = D_adcb3*0.05 * 0.36632;;
     if (D > 1125)
     {D =1125;
     }}
     else
     { D = 4999-(D_adcb3*0.05 * 0.36632);;
     if (D < 4249)
     {D =4249;
     }}

    EPwm2Regs.TBPHS.bit.TBPHS = D1;
    EPwm4Regs.TBPHS.bit.TBPHS = D;
    EPwm5Regs.TBPHS.bit.TBPHS = D+D2;
    //EPwm6Regs.TBPHS.bit.TBPHS = D2;

     //
     // Clear INT flag for this timer
     //
         AdcbRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; //clear INT2 flag
     //
     //


    //
    // Acknowledge this interrupt to receive more interrupts from group 3
    //
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP10;
}

//
// InitEPwm1Example - Initialize EPWM1 configuration
//
void InitEPwm1Example()
{
    EPwm1Regs.TBPRD = 4999;                       // Set timer period
    EPwm1Regs.TBPHS.bit.TBPHS = 0x0000;           // Phase is 0
    EPwm1Regs.TBCTR = 0x0000;                     // Clear counter

    //
    // Setup TBCLK
    //
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; // Count down
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;        // Disable phase loading
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;

    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Setup compare
    //
    EPwm1Regs.CMPA.bit.CMPA = 2500;

    //
    // Set actions
    //
    EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR;            // Set PWM1A on CMPA and reset at ZRO
    EPwm1Regs.AQCTLA.bit.CAD = AQ_SET;

    //
    // Active High Complementary
    //
    EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;      // Disable deadband since gate driver have its own
    EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    EPwm1Regs.DBRED.bit.DBRED = EPWM_DB;
    EPwm1Regs.DBFED.bit.DBFED = EPWM_DB;

/*    //
       // start SOC
       //
        EPwm1Regs.ETSEL.bit.SOCAEN    = 0;    // Disable SOC on A group
        EPwm1Regs.ETSEL.bit.SOCASEL   = 5;   // Select SOC on down-count
        EPwm1Regs.ETPS.bit.SOCAPRD    = 1;       // Generate pulse on 1st event
        EPwm1Regs.TBCTL.bit.CTRMODE   = TB_FREEZE; // FREEZE
*/

}

//
// InitEPwm2Example - Initialize EPWM2 configuration
//
void InitEPwm2Example()
{
    EPwm2Regs.TBPRD = 4999;                       // Set timer period
    EPwm2Regs.TBPHS.bit.TBPHS = 2500;               // Phase is 0
    EPwm2Regs.TBCTR = 0x0000;                     // Clear counter

    //
    // Setup TBCLK
    //
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; // Count down
    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;        // Disable phase loading
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;

    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
    EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Setup compare
    //
    EPwm2Regs.CMPA.bit.CMPA = 2500;

    //
    // Set actions
    //
    EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR;            // Set PWM2A on Zero
    EPwm2Regs.AQCTLA.bit.CAD = AQ_SET;

    //
    // Active High Complementary
    //
    EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
    EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    EPwm2Regs.DBRED.bit.DBRED = EPWM_DB;
    EPwm2Regs.DBFED.bit.DBFED = EPWM_DB;
}

// EPWM3 will be unused.
// InitEPwm3Example - Initialize EPWM2 configuration
//
void InitEPwm3Example()
{
    EPwm3Regs.TBPRD = 1249;                       // Set timer period
    EPwm3Regs.TBPHS.bit.TBPHS = 0x0000;                // Phase is 0
    EPwm3Regs.TBCTR = 0x0000;                     // Clear counter

    //
    // Setup TBCLK
    //
    EPwm3Regs.TBCTL.bit.PHSEN = TB_ENABLE;        // Disable phase loading
    EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;

    EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
    EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm3Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm3Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Setup compare
    //
    EPwm3Regs.CMPA.bit.CMPA = 625;

    //
    // Set actions
    //
    EPwm3Regs.AQCTLA.bit.ZRO = AQ_CLEAR;            // Set PWM1A on Zero
    EPwm3Regs.AQCTLA.bit.CAD = AQ_SET;

    //
    // Active High Complementary
    //
    EPwm3Regs.DBCTL.bit.OUT_MODE = DB_DISABLE;
    //EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    //EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    //EPwm3Regs.DBRED.bit.DBRED = EPWM_DB;
    //EPwm3Regs.DBFED.bit.DBFED = EPWM_DB;

    //
   // start SOC
   //
    EPwm3Regs.ETSEL.bit.SOCAEN    = 0;    // Disable SOC on A group
    EPwm3Regs.ETSEL.bit.SOCASEL    = 5;   // Select SOC on down-count
    EPwm3Regs.ETPS.bit.SOCAPRD = 1;       // Generate pulse on 1st event
    EPwm3Regs.TBCTL.bit.CTRMODE = TB_FREEZE; // FREEZE
}

//
// InitEPwm4Example - Initialize EPWM2 configuration
//
void InitEPwm4Example()
{
    SyncSocRegs.SYNCSELECT.bit.EPWM4SYNCIN = 0;   //EPWM1SYNCOUT
    EPwm4Regs.TBPRD = 4999;                       // Set timer period
    EPwm4Regs.TBPHS.bit.TBPHS = 0;           // Phase is D
    EPwm4Regs.TBCTR = 0x0000;                     // Clear counter

    //
    // Setup TBCLK
    //
    EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN; // Count down
    EPwm4Regs.TBCTL.bit.PHSEN = TB_ENABLE;        // Disable phase loading
    EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN;   //It should be set to zero

    EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
    EPwm4Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm4Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm4Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Setup compare
    //
    EPwm4Regs.CMPA.bit.CMPA = 2500;

    //
    // Set actions
    //
    EPwm4Regs.AQCTLA.bit.ZRO = AQ_CLEAR;            // Set PWM4A on Zero
    EPwm4Regs.AQCTLA.bit.CAD = AQ_SET;


    //
    // Active High Complementary
    //
    EPwm4Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
    EPwm4Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    EPwm4Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    EPwm4Regs.DBRED.bit.DBRED = EPWM_DB;
    EPwm4Regs.DBFED.bit.DBFED = EPWM_DB;
}

//
// InitEPwm5Example - Initialize EPWM2 configuration
//
void InitEPwm5Example()
{
    EPwm5Regs.TBPRD = 4999;                       // Set timer period
    EPwm5Regs.TBPHS.bit.TBPHS = 0;               // Phase is D
    EPwm5Regs.TBCTR = 0x0000;                     // Clear counter

    //
    // Setup TBCLK
    //
    EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_DOWN;  // Count down
    EPwm5Regs.TBCTL.bit.PHSEN = TB_ENABLE;        // Disable phase loading
    EPwm5Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;       // Clock ratio to SYSCLKOUT
    EPwm5Regs.TBCTL.bit.CLKDIV = TB_DIV1;
    EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;

    EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;    // Load registers every ZERO
    EPwm5Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm5Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm5Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Setup compare
    //
    EPwm5Regs.CMPA.bit.CMPA = 2500;

    //
    // Set actions
    //
    EPwm5Regs.AQCTLA.bit.ZRO = AQ_CLEAR;            // Set PWM1A on Zero
    EPwm5Regs.AQCTLA.bit.CAD = AQ_SET;

    //
    // Active High Complementary
    //
    EPwm5Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
    EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
    EPwm5Regs.DBCTL.bit.IN_MODE = DBA_ALL;
    EPwm5Regs.DBRED.bit.DBRED = EPWM_DB;                 //2 us..... since EPWMCLK = TBCLK/1
    EPwm5Regs.DBFED.bit.DBFED = EPWM_DB;
}


void ConfigureADC(void)
{
    EALLOW;

    //
    //write configurations
    //

    AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
    AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);

    //
    //Set pulse positions to late
    //
    AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;

    //
    //power up the ADCs
    //
    AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;

    //
    //delay for 1ms to allow ADC time to power up
    //
    DELAY_US(1000);

    EDIS;
}

//
// SetupADCSoftware - Setup ADC channels and acquisition window
//
void SetupADCSoftware(void)
{
    Uint16 acqps;

    //
    // Determine minimum acquisition window (in SYSCLKS) based on resolution
    //
    if(ADC_RESOLUTION_12BIT == AdcbRegs.ADCCTL2.bit.RESOLUTION)
    {
        acqps = 20; //75ns
    }
    else //resolution is 16-bit
    {
        acqps = 63; //320ns
    }

    if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
        {
            acqps = 20; //75ns
        }
        else //resolution is 16-bit
        {
            acqps = 63; //320ns
        }

    //
    //Select the channels to convert and end of conversion flag
    //ADCB
    //
    EALLOW;
    AdcaRegs.ADCSOC0CTL.bit.CHSEL = 2;  //SOC0 will convert pin A2
    AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps +
    AdcaRegs.ADCSOC0CTL.bit.TRIGSEL =9;     //1 SYSCLK cycles

    AdcaRegs.ADCSOC1CTL.bit.CHSEL = 3;  //SOC1 will convert pin A3
    AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps +
    AdcaRegs.ADCSOC1CTL.bit.TRIGSEL =9;     //1 SYSCLK cycles

    AdcbRegs.ADCSOC2CTL.bit.CHSEL = 2;  //SOC2 will convert pin B2
    AdcbRegs.ADCSOC2CTL.bit.ACQPS = acqps; //sample window is acqps +
    AdcbRegs.ADCSOC2CTL.bit.TRIGSEL =9;     //1 SYSCLK cycles

    AdcbRegs.ADCSOC3CTL.bit.CHSEL = 3;  //SOC2 will convert pin B3
    AdcbRegs.ADCSOC3CTL.bit.ACQPS = acqps; //sample window is acqps +
    AdcbRegs.ADCSOC3CTL.bit.TRIGSEL =9;     //1 SYSCLK cycles


    AdcbRegs.ADCINTSEL1N2.bit.INT2SEL = 0x3; //end of SOC1 of Adcb will set INT2 flag
    AdcbRegs.ADCINTSEL1N2.bit.INT2E = 1;   //enable INT2 flag
    AdcbRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; //make sure INT2 flag is cleared
    EDIS;
}
//
// End of file
//

I am really suffering from a long time. Hope you can help me in this regard!! Thanks in advance
Sayandev

  • Hi Sayandev,

    I didn't fully understand your code, but are you sure that this is implementing a moving average?  It seems like the control variables in the ADC ISR only get updated when the buffer fills up (e.g. when indexD12 >= D12_BUFFER, then D1 and D2 change value).  I think for a moving average you'd add the new value to a sum each ISR while also subtracting out the oldest value. 

    On the ADC side, it looks like you are using the minimum S+H (set by ACQPS) time.  This would be appropriate if you have a very good ADC input driver (high bandwidth op-amp + series R of maybe 10-100 ohms and C value of ot more than a couple 100pF), otherwise you may need a longer value.  See https://www.ti.com/lit/an/spract6/spract6.pdf for more information.  Adding slightly more aggressive low-pass filtering on the ADC input might help with your noise issues, but would probably require additional S+H time (or you can build a separate filter stage in the ADC signal conditioning circuits if you also need to use a short S+H time).       

  • Sorry for the inconvenience. It was not moving average, rather only averaging. I will look into S+H time.