Part Number: TMS320F280025C
Hello,
I'm making ePWM module for 0% to 100% duty cycle control at Up-Count mode.
The following is an excerpt.
When I set up the following program, the duty cycle becomes 100% only the first time after the microcontroller starts.
init_func()
EPwm1Regs.TBCTL.bit.CTRMODE = 3; /* stop */
EPwm1Regs.TBPRD = 1000; /* 100kHz */
EPwm1Regs.AQCTL.bit.SHDWAQAMODE = 1; /* shadow ON */
EPwm1Regs.AQCTL.bit.LDAQAMODE = 0; /* reload =zero*/
EPwm1Regs.CMPA.bit.CMPA = 700; /* initial duty 70% */
~~~~~~~~~~~~~~~
start_func()
EPwm1Regs.AQCTLA.bit.CAU = 1; /* clear */
EPwm1Regs.AQCTLA.bit.ZRO = 2; /* set */
EPwm1Regs.TBCTL.bit.CTRMODE = 0; /* start */

My expectation is that the first waveform will output about 70% duty.
However, the behavior was different from my expectation.
"EPwm1Regs.AQCTLA.bit.CAU" seems to be ignored the first time, what is the cause?
Is it the shadow mode of the AQ sub-module that is causing the problem, or is it the priority of "EPwm1Regs.TBCTL.bit.CTRMODE = 3" that is affecting it?
<supplement>
I understood I can get around this by "turning off the shadow mode of AQ sub-module" or "starting the TBCTL counter before setting the AQCTLA".
However, I would like to know the true cause mentioned above.
Best regards,
Masaru Maeda,