Part Number: TMS320F28023
Other Parts Discussed in Thread: C2000WARE, TMS320F280023,
Can I get full fledged FLASH .cmd file for this processor ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28023
Other Parts Discussed in Thread: C2000WARE, TMS320F280023,
Can I get full fledged FLASH .cmd file for this processor ?
Hi,
What do you mean by a full fledged Flash command file? There are a couple of linker command files provided in C2000Ware for F2802x devices - F28023.cmd and F2802x_generic_flash.cmd files which you can refer.
Best Regards
Siddharth
Looks at the piccolo .cmd file below that utilizes IQmath and _IQmath Tables and I use it for F28027 piccolo processor.
However, I do NOT see any .cmd FLASH in C2000Ware that has _IQmath for TMS320F280023 processor !! Let me know how to utilize FPU, FINTDIV, TMU units in this processor as well,
///////////////////////////////////////////////////////////////PICCOLO//////////////////////////////////////////////////////////////////////////////
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
PRAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHA : origin = 0x3F7000, length = 0x000F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASH. CSM password locations in FLASHA */
FLASHB : origin = 0x3F6000, length = 0x001000 /* on-chip FLASH */
FLASHC : origin = 0x3F5000, length = 0x001000 /* on-chip FLASH */
FLASHD : origin = 0x3F4000, length = 0x001000 /* on-chp FLASH */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
DRAML0 : origin = 0x008800, length = 0x000800 /* on-chip RAM block L0 */
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHD, PAGE = 0
.pinit : > FLASHA, PAGE = 0
.text : >> FLASHA | FLASHB | FLASHC | FLASHD, PAGE = 0
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHA,
RUN = PRAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > DRAML0 PAGE = 1
.esysmem : > DRAML0 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
Hi,
The file F28023.cmd does have the IQMath entries, it is located in <C2000WareInstallDir>\device_support\f2802x\common\cmd folder.
Best Regards
Siddharth
Hi,
Got confused since you mentioned the device as "TMS320F28023". You can use the linker cmd file "28002x_generic_flash_lnk" located in <C2000WareInstallDir>\device_support\f28002x\common\cmd folder and change the following lines
/* Allocate IQ math areas: */
IQmath : > FLASH_BANK0_SEC1, ALIGN(8)
IQmathTables : > FLASH_BANK0_SEC2, ALIGN(8)
Best Regards
Siddharth
thanks Siddharth for responding,
Further questions:
1. Do I need to specify the BOOT ROM memory location of IQTABLE in "28002x_generic_flash_lnk" as did in "PICCOLO" as following ?
/////////////////////////////////////////////////////////////////////////////////
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
//////////////////////////////////////////////////////////////////////////////////
or just "BOOTROM: origin = 0x003F0000, length = 0x00008000" in "28002x_generic_flash_lnk" is good enough. Can you explain this ?
2. How do I utilize FPU, FINTDIV, TMU units in F280023 uC ? pl. guide.
3. Do you have any sample code utilizing FPU, FINTDIV, TMU units in F280023 uC ?
Hi,
1. You can refer the TRM section "Boot ROM Memory Maps" and define the IQTABLES in the linker command
2. You can enable the compiler options in the project to utilize the --float_support=fpu32 --tmu_support=tmu0 and use compiler instrincs in your code
Refer the compiler user guide section 7.6 www.ti.com/.../spru514w.pdf
3. You can take a look at the examples provided in C2000Ware . For each library , there are few examples provided.
Best Regards
Siddharth