This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2809: Question about Peripheral Frame 0

Part Number: TMS320F2809

Dear team:

In the ADC documentation Page 44, there are the following:

In the cascaded sequencer mode, registers ADCRESULT8 through ADCRESULT15 holds the results of the ninth through sixteenth conversions. The ADCRESULTn registers are left justified when read from Peripheral Frame 2 (0x7108-0x7117) with two wait states and right justified when read from Peripheral Frame 0 (0x0B00-0x0B0F) with zero wait states.

The customer finds that the address of his ADCRESULTn register is located in Peripheral Frame 2. How should I set it so that the address of the ADCRESULTn register is located in Peripheral Frame 0 (0x0B00-0x0B0F) to reduce 2 waiting cycles?

Best regards