Part Number: DRV8301-69M-KIT
I am working with Simulink for the generation of the code for the microproccesor, and I want to generate a code that executes standalone, as soon as I turn on the device. My main problem is that, once I swicth on the device, the program does not run, but if I connect de microusb and disconect ti (the one I am using for programing), the code suddenly stars running.
How could I achive running the code without needing to connect and disconnect the usb?
I attach you the some info about how am I using the system:
-Device power supply: I am using the internal voltage coonverter to supply both the HV circuitry and the Control Board. (PVDD 24 V)
-Hardware configuration in Simulink: The box Boot from flash checked
- Control Board Configuration: SW1 in ON position 1 and position 2
Thank you in advance.