This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT: Noisy running Level5

Part Number: TMDSHVMTRPFCKIT


Dear team:

My customer is using the R1.1 version of the kit to control the operation of the motor, using a servo motor control routine.
In Level5, when RunMotor=1 is set, the motor rotates, but there is a lot of noise, which is completely different from the previous test module. There was almost no noise during the previous speed test, but the position test was very loud. What is the reason?

Best regards