Part Number: CCSTUDIO-C2000
I got a compile error with CCSv11 for my old C2000 project (used to use CCSv5.3).
I saw this thread e2e.ti.com/.../2046257 talking about the same error "Product XDAIS v0.0 is not currently installed and no compatible version is available. Please install this product or a compatible version." The solution was to remove the XDAIS under Property->General->Production tab. But mine doesn't have Products tab, how do I remove the reference to XDAIS? I have deleted XDAIS_CG_ROOT from Project Properties->Build->C2000 Compiler->Include Options and didn't help
.