Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28069
I am planning on using a F28069 in my project. I got the eval kit and control card for the F28069. When I try to run the example from controlSUITE cla_adc_fir_flash I get an error when trying to load code into the device. The error reads:
C28xx: Flash Programmer: Unable to read algorithm file (C:\Program Files (x86)\Texas Instruments\ccsv4\DebugServer\bin\win32\..\..\..\C2000\flashAlgorithms\FlashAPIInterface2806xV1_00.out). Operation cancelled.
C28xx: Flash Programmer: Error erasing Flash memory.
The examples that run out of RAM work fine. If I swap the control card for the F28035, the same example for the F28035 works without any trouble.
Does anyone know what the algorithm file is about?
Thanks,
Ethan