This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

flash code problem after power on reset

hi

I am using ccs3.3 bios 5.33.06, dsc f28335, i have followed spra 958i ,i was able to run motor control code from ti (modified)  from ram with pwm at 10khz , when i have changed my code to run from flash it runs ok as long as i am not doing power on reset. when i do power on reset i cant see my pwm on scope which i could see before resetting it. f28335 control card has gpio 84,85,86,87 as pulled up which is for boot to flash mode. also i found that if i am not servcing pwm interrupt as it occurs and i only toggle a gpio in a while loop i can see gpio toggling even after power on reset from flash. 

Please help me in this regard

Ahmed Shakeel