Hi
I am using a demo code "hrpwm_ex2_prdupdown_sfo_v8" and tried to generate a PWM @ 585.XXHz. I used a function HRPWM_Config(10667) and change below parameter from
(*ePWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV1;
(*ePWM[j]).TBCTL.bit.CLKDIV = TB_DIV1; // TBCLK = SYSCLKOUT
to
(*ePWM[j]).TBCTL.bit.HSPCLKDIV = TB_DIV4;
(*ePWM[j]).TBCTL.bit.CLKDIV = TB_DIV4; // TBCLK = SYSCLKOUT
However, EPWM1A is always 100% duty. I have tried different parameters. Only using original parameter can generate PWM @ 4.96KHz. Please advise do I miss something.
BR
HK Woo