Part Number: TMS320F280049
1. what is the difference between initsyspll vs sysctrl_setclock?
2. I am using ASEMB-14.7256MHZ-LC-T, which is a single ended clock input. When setting system clock, i noticed both XTAL_OSC_SE or XTAL_OSC works. why?
3. I am modifying TIDM_DC_DC_BUCK software, after setting up the clock, there are two ASSERT as shown. If the expression is false, what is the reaction of the program? When i am debugging, even the expression is false, I am still able to step through the program, why?
3.