This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem in connecting to F28335 eZdsp target board



Hi all,

I am trying to connect to F28335 eZdsp target board using USB cable and getting the following error message:

Error connecting to the target:
Error 0x80000200/-1135
Fatal Error during: OCS,
Unrecoverable emulation error

Sequence ID: 0
Error Code: -1135
Error Class: 0x80000200
I/O Port = 540

Board Name: F28335_eZdsp
Cpu Name: cpu_0

I tried to connect with another working board and it works fine. It seems like problem with the new board.

Please provide any solution if you have!!!!!

Thank you

JJ