Part Number: TMS320F28377D
Other Parts Discussed in Thread: TEST2
As mentioned in the manual,in order to allow multiple comparators at a time to affect DCA/BEVTx events and trip actions, there is a OR logic to bring together ALL trip inputs (up to 15) from sources external to the ePWM module.In order to achieve this function, I configured the relevant registers and did experiments,through the test, I found the following phenomenon:
1)If the default polarity of the input signal is high and the abnormal polarity is low, then all signals need to be low to generate DCA/BEVTx events.This does not accord with the description in the manual.
2)If the signal default polarity is low and abnormal is high, then, one signal is high can generated DCA/BEVTx events.This is consistent with the description in the manual.
So, I would like to confirm whether the use of OR logic requires polarity of input signals.
Looking forward to your reply.