Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE-MOTORCONTROL-SDK, C2000WARE
I use your enhanced sliding mode observer (ESMO) for controlling a PMSM motor. It works well when I start the motor. As the motor heats up (I think this is the cause), the speed goes down. I suspect the increase in the stator resistance causes this. To understand what is going on, we bought the hardware that can run InstaSPIN. With InstaSPIN, we do not see this issue. So, I have the following questions.
1. Does InstaSPIN use ESMO or some other control method?
2. I understand InstaSPIN does some adaptive stuff. Does it compensate only for changes in the stator resistance?
3. InstaSPIN library is available in Q-Math. Can we get a floating point version that runs on F28377x?
4. I can get very accurate rotor angle estimations using Hall sensor data and a Kalman filter. Do you think the InstaSPIN adaptive mechanism will be as robust as that? I assume you have done an accuracy check of the estimated angle as the parameter changes.
Thanks very much,
Dhammika